LTE employs a new network architecture made up of multiple Evolved Packet Cores (EPCs) that communicate with each other and with evolved universal terrestrial radio access network base stations (eNBs). Each EPC contains a Mobile Management Entity (MME) and a System Architecture Evolution Gateway (SAE). The eNB stations communicate with the EPCs, with each other, and with user equipment (UE).
Click Uplink in the tree view to open the Uplink node. The Uplink node enables you to set cell parameters and sounding reference signal parameters.
|
Uplink |
|---|
Click the Predefined Configuration button
to access a dialog box
from which you can select a base channel configuration.
Click the click the Wizard button
to open the UL RMC Wizard.